Create a login form

Create an interface that allows for logging in.
  1. Add a preconfigured widget (type):
    1. In the toolbar, select
      Template Libraries
      .
    2. In , search for
      Login form
      .
    3. Under
      Components
      , drag
      Login form
      onto
      UI
      in
      Project view
      .
  2. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    LoginForm1
    LoginFormComponents
    Login
    .
  3. In
    Properties
    , create a dynamic link between
    Users
    and
    ProjectName
    Security
    Users
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.