Develop the subscriber NetLogic and interface

Develop a NetLogic and integrate it with the interface.
  1. Develop the NetLogic
  2. Right-click
    MainWindow (type)
    and select
    New
    Runtime NetLogic
    .
  3. Hover-over the NetLogic, select
    Edit
    , and enter
    SubscriberLogic
    .
  4. Double-click the NetLogic.
    The external code editor opens.
  5. In the code editor, replace the existing code with the following code:
    #region StandardUsing using System; using FTOptix.CoreBase; using FTOptix.HMIProject; using UAManagedCore; using OpcUa = UAManagedCore.OpcUa; using FTOptix.NetLogic; using FTOptix.UI; using FTOptix.OPCUAServer; #endregion using uPLibrary.Networking.M2Mqtt; using uPLibrary.Networking.M2Mqtt.Messages; public class SubscriberLogic : BaseNetLogic { public override void Start() { var brokerIpAddressVariable = Project.Current.GetVariable("Model/BrokerIpAddress"); // Create a client connecting to the broker (default port is 1883) subscribeClient = new MqttClient(brokerIpAddressVariable.Value); // Connect to the broker subscribeClient.Connect("
    SubscriberClient
    "); // Assign a callback to be executed when a message is received from the broker subscribeClient.MqttMsgPublishReceived += SubscribeClientMqttMsgPublishReceived; // Subscribe to the "my_topic" topic with QoS 2 ushort msgId = subscribeClient.Subscribe(new string[] { "/my_topic" }, // topic new byte[] { MqttMsgBase.QOS_LEVEL_EXACTLY_ONCE }); // QoS level messageVariable = Project.Current.GetVariable("Model/Message"); } public override void Stop() { subscribeClient.Unsubscribe(new string[] { "/my_topic" }); subscribeClient.Disconnect(); } private void SubscribeClientMqttMsgPublishReceived(object sender, MqttMsgPublishEventArgs e) { messageVariable.Value = "Message received: " + System.Text.Encoding.UTF8.GetString(e.Message); } private MqttClient subscribeClient; private IUAVariable messageVariable; }
  6. Save the code.
  7. Create the interface elements
  8. Create the message variable by performing the following actions:
    1. In
      Project view
      , right-click
      Model
      and select
      New
      Variable
      .
    2. Hover-over the variable, select
      Edit
      , and enter
      Message
      .
    3. In
      Properties
      , select
      Int32
      and select
      String
      .
  9. Create the Subscribe label by performing the following actions:
    1. In
      Project view
      , right-click
      MainWindow (type)
      and select
      New
      Base controls
      Label
      .
    2. Hover-over the label, select
      Edit
      , and enter
      SubscribeLabel
      .
    3. In
      Properties
      , create a dynamic link between
      Text
      and the
      Message
      variable.
      For more information about dynamic links, see Create dynamic links.
  10. Arrange the interface elements.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.