Create application logic
Create a dynamic link between the label and either the ClockLogic or System object.
- InProject view, selectDateTimeLabel.
- InProperties, create a dynamic link betweenTextand either:
- .
- .
- .
For more information about dynamic links, see Create dynamic links.TIP:While creating the dynamic link, useFormatto select a different date and time format.If you get time from ClockLogic, you can expand theTimeorUTCTimenodes to accessYear,Month,Day,Hour,Minute, andSecondvariables.
Provide Feedback