Select Channels to Calibrate

To select channels to calibrate:
  1. Select the
    Calibrate?
    box for each channel that you want to calibrate.
  2. Select the desired method of calibration button (
    Groups
    or
    One at a Time
    ).
    You can calibrate channels in groups at the same range simultaneously, or one at a time. When you calibrate channels one at a time, you go through a complete calibration on a per channel basis before moving onto calibrate the next channel.
  3. Select:
    • Back
      to return to the previous screen.
    • Next
      to continue.
    • Stop
      to cancel the calibration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.