- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Equipment Sequence Monitor
Open the by opening an is the routine window.
Equipment Sequence
MonitorEquipment Sequence
diagram from the Controller Organizer
or Logical Organizer
, and going on line with the controller. The Equipment Sequence
MonitorThe
Equipment Sequence
Monitor is the online version of the Equipment Sequence
Editor and is used to monitor and interact with Equipment Sequences that have been downloaded to the controller. The control engineer can do the following: - Command the Equipment Sequence.
- Change the value of parameters and attributes.
- Interact with the executing sequence.
Provide Feedback