Import/Paste Configuration dialog box - Routines tab settings
The following information describes imported local tags on the
Import Configuration - Routines
dialog box.Setting | Description | ||||||||
---|---|---|---|---|---|---|---|---|---|
Row Header | The leftmost part of the grid provides an indication of the condition of the component that was imported, as follows:
| ||||||||
Import Name | Displays the name of the component as read from the import file. An import name appears only for tags that exist in both the project and in the import content. | ||||||||
Operation | Displays the operation for each tag dependent upon the operation selected for the routine being imported:
| ||||||||
Differences ![]() | Icon changes to provide at-a-glance indications of how the imported content matches the project content, as follows:
| ||||||||
Final Name | Displays the contents of the Import Name box, unless Operation is set to Discard or the routine exists in the project but not in the import content (the Import Name is blank).For cases where the routine exists in the project but not in the import content, this box contains the name of the routine in the project. | ||||||||
Type | Displays the routine type of the displayed component from the import content. | ||||||||
Collision Details / Properties | If the imported routine collides with an existing routine in the project, the Collision Details button appears in this column. Click the Collision Details button to open the Collision Details dialog box.If the routine does not collide with a component, the Properties button appears in this column. Click Properties to open the Properties dialog box. | ||||||||
Description | Displays the description of the displayed component. |
Provide Feedback