Temporarily Hide/Show Actions command

Choose this command to alternately display or hide the actions associated with the selected step. As the command name implies, this option is temporary and the setting is not saved to the controller or to the offline project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.