Overview
In this webinar, participants will get the necessary details to be able to configure the FactoryTalk (FT) Optix connector, which serves as an interface to connect and transfer data from FT Optix into FactoryTalk DataMosaix. We will be using a Rockwell Automation controller as a data source for demonstration, however, the concept can be used with third party data sources. We will explain the difference between FT Optix connector and the FT Optix OPC UA extractor. Our focus will be in transferring data from FT Optix into FactoryTalk DataMosaix.
What you will learn
Speakers