MES in the Cloud Offers Scale and Reliability
Whether MES is an integral part of the corporate backbone or a separate, best-in-class addition, cloud deployment makes sense for several reasons. Uptime for plant operations is critical and if the enterprise system is down for planned or unplanned maintenance, the plant cannot function.
Manufacturers can look to Plex Systems, a Rockwell Automation company that provides a Smart Manufacturing Platform as a solution. The software-as-a-service, cloud-native smart manufacturing platform offers the flexibility to connect, automate, track, and analyze – the four key capabilities required of manufacturers and Industry 4.0. It includes options for MES, ERP, supply chain planning and management, quality, Industrial IoT (IIoT) and analytics.
With cloud deployment – especially true with SaaS – all maintenance and support are handled by an organization whose core competence is to keep the system up and running. Moreover, some cloud solutions continuously deploy enhancements and fixes so there is no need to take down the system for upgrades. If a service interruption occurs, there are always live back-up (hot site) facilities available.
In addition, as economies and markets rise and fall, IT resources to support plant expansion and contraction are scalable instantly without significant IT investment or involvement.
With effective integration between the relevant data streams, plants can configure and reconfigure their MES system to suit their needs without impact on the parent ERP system. Configuration and testing are done “offline” and when the system is ready to be deployed, it happens with a flick of a switch. Moreover, in support of the goal of MES standardization, subsequent plants can be brought online using the same configurations in a fraction of the time and create a standard configuration across the enterprise to make management more effective.
Since the industrial automation network is connected to physical hardware and must support lots of data at potentially high speeds, it has traditionally been supported by an on-premise server. Data is communicated to the MES as required and with cloud MES, synchronizes using that edge server.
MES offers tight control of the various aspects of production including recording of uptime, production, and scrap. With a cloud deployment, remote supervisors can easily access all data regarding production, inventory and quality via mobile devices and the Internet. This enables managers to quickly engage in urgent issues whether they are on the other side of the plant or on the other side of the planet.
Quality managers can monitor, react and make immediate decisions to isolate and contain potential quality risks before they “escape” and result in chargebacks or worse – a recall. If there is a quality issue result, traceability to potential failure points can swiftly uncover the culprit – even if caused by an upstream supplier – and enable quick resolution and reporting. Most importantly, this information is available in real time from anywhere through a simple Internet connection.
Moving to the Cloud
A growing number of manufacturers are relying on cloud-based MES solutions to help manage their business because of this flexibility and the ability to be much more responsive to plant floor activities.
Cloud deployment and SaaS proven to be effective strategies for ERP. A rapidly growing number of enterprises opting for the cloud as the preferred platform for their enterprise system. These same benefits are available for cloud-based MES.
Cloud/SaaS allows the manufacturer to focus on high-value activities like designing, manufacturing and distributing product by off-loading the IT burden while eliminating any worries about support, security and keeping the systems up-to-date and productive.
As companies grow and expand, they can do so more easily without the traditional expansion of IT footprint, budget, and staff and can focus their resources on their core competency – production. Moreover, valuable technical professionals – difficult to find in today’s tight labor market – can be redirected to focus on more strategic pursuits such as spending more time with data and process analysis.
It is the perfect complement to the growth of IIoT, helping to gather, connect and analyze virtually any data from production operations to drive greater operational efficiency.