Chart Types

Chart Types

The following are the list of chart types:
NOTE:
When Direct Query is enabled the “Multi X Bar Chart” and “Multi X Line Chart” are not supported.
“Bar Charts"
  • "Basic Bar Chart”
  • “Multi Color Bar Chart”
  • “Multi X Bar Chart”
  • “Inverted Bar Chart”
  • “Stacked Bar Chart”
  • “Inverted Stacked Bar Chart”
  • “Bar Time Series Chart”
“Pie Charts”
  • “Basic Pie Chart”
  • “Donut Pie Chart”
  • “Semi Circle Pie Chart”
“Gauge Charts”
  • “Semi Circle Gauge Chart”
  • “Full Circle Gauge Chart”
  • “Bourdon Gauge Chart”
“Line Charts”
  • "Basic Line Chart”
  • “Multi X Line Chart”
  • “Line Time Series Chart”
“Pareto Chart”
“Combination Chart”
“Text Chart”
“Metric Chart”
“Heatmap Chart”
Chart Type
NOTE:
Once a chart is created with a set title, the change in the X axis and Y axis settings under the configuration tab does not affect the chart title.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal