Configure a momentary button
- InProject view, right-click a node to contain the button and select .For example, add the button underMainWindow (type).
- (optional) InProject view, hover-over the button, select , and enter a new name for the button.
- (optional) InProperties, adjust the button look and feel:
- Appearance. Adjust the button visibility, state, opacity, rotation, background color, and style.
- Size and layout. Adjust the button size and position in your project.
- Text and font. Enter the text to display in the button and adjust the text style.
- Image. Include an icon inside the button and decide where to place the icon in relation to the button text.TIP: SelectBrowseand then either selectImport file(s)Image positionto align the image in relation to the button text.
- InEvents, create dynamic links between specific events and methods to execute.For more information about the available events, see Momentary button.
momentary
momentary button
Provide Feedback