Definitions, acronyms, and abbreviations

Definitions, acronyms, and abbreviations
Term
Definition
PCDC
The Product Compatibility and Download Center (PCDC) can help you find product-related downloads including firmware, release notes, associated software, drivers, tools and utilities. http://www.rockwellautomation.com/rockwellautomation/support/pcdc.page
AOP
Add on Profiles. An Add on Profile is used within Studio 5000 to define a specific piece of hardware and how it will react within the control system.
Air gap
Air gap is a network security measure employed on one or more computers to ensure that a secure computer network is physically isolated from unsecured networks.
Normal mode
In FactoryTalk Updater, it is a default mode that FactoryTalk Updater will collects installed software information, static and transaction activation information, AOP information in agent, and get and show the latest information of installed software from PCDC and do the patch deployment just like the previous version.
OT mode
OT (Operational technology) is hardware and software that detects or causes a change, through the direct monitoring and/or control of industrial equipment, assets, processes and events. OT environment usually describes environments containing industrial control systems (ICS). In FactoryTalk Updater, it refers to the environment that cannot connect to PCDC.
IT mode
IT (Information technology) is the use of computers to create, process, store, retrieve and exchange all kinds of data and information. In FactoryTalk Updater, it refers to the environment that can connect to PCDC
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.