Installation from screens
FactoryTalk Updater versions 3.00.00 and later use Windows authentication to enhance product security. This requires FactoryTalk Agent and FactoryTalk Server machines to be in the same domain. A stand-alone installation to a computer may be a domain or workstation. Installation can be done via screens or scripted commands documented at Release Notes>Application Notes.
The FTU Agent should be installed on all computers of interest within a network. The FTU Agent collects information from the local computer for the FTU Server. One FTU Server is needed on the network to collect and persist information. The FTUpdater Collector is optional and is installed disabled. At least one FTU Client is needed on the network to connect to FTU Server and configure the system.
Provide Feedback