Perform manual installation

Use a custom installation to install more than one FactoryTalk Updater functionality.
Download the current version of FactoryTalk Updater software.
  1. Launch
    Setup.exe
    .
  2. In
    Select product to install
    , select one of these options: Agent, Server, Client, Custom Installation.
  3. Select
    Install now
    .
  4. Read and consent to the End User License Agreements by selecting
    Accept all
    .
    The installation starts and a bar displays the progress.
  5. When prompted to restart the computer, select
    Restart now
    .
  6. Perform one of the following actions:
    • To exit the installation, select
      Close
      .
    • To see the installation details, select
      Installation Summary
      .
    • To learn how to receive email updates about product patches, select
      Register for updates
      .
    • To install Adobe Acrobat Reader, select
      Download it free
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.