System requirements

Hardware requirements

FactoryTalk Updater does not have any specific hardware requirements. It runs on any hardware platform that supports the required software, either locally or on a virtual machine.
Rockwell Automation recommends at least 80 MB of available drive space for FactoryTalk Updater.

Software requirements

  • FactoryTalk Updater runs on these Windows® operating systems:
    • Windows 10 Professional Edition 64-bit
    • Windows 10 Enterprise Edition 64-bit 
    • Windows 10 Enterprise 2019 LTSC(1809)
    • Windows 10 Enterprise 2021 LTSC 64-bit (21H2)
    • Windows 11 Enterprise 64-bit
    • Windows 11 Professional 64-bit
    • Windows Server® 2019 Standard
    • Windows Server 2019 DataCenter
    • Windows Server 2022 DataCenter
    • Windows Server 2022 Standard
    TIP: The installer software inhibits installation of FactoryTalk Updater on all Windows 7 and 32-bit operating systems, including Windows 10 (32 bit).
  • Internet browsers:
    • Edge™
    • FactoryTalk Updater web client: Chrome™ browser 
    • FactoryTalk Updater web client: Firefox®
  • When you install FactoryTalk Updater, if it is not already present, the following software is installed:
    • .NET Framework 4.8
    • Rockwell Software Windows Firewall Configuration Utility 1.00.16
    • Microsoft .NET Hosting v6.0.4.22172 and IIS URL Rewrite Module v7.2.1993
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.