Information displayed in the Machines view
Select the Machines icon in the view menu to display a list of all machines or a list of machines in a group. Enter a search term in the Search box to highlight that term in the list.
Column | Description |
---|---|
Name | The name of the machine. Select the expand icon to display the list of monitored software installed on the machine. Select the expand icon for each software application to display installed versions and utilities. Tip: The Name box displays only the first 15 characters in the machine name. Names longer than 15 characters are truncated. |
Address | The IP address of the machine. |
Status | The online or offline status of the machine. |
Installed version | The installed version of software. The Version Lifecycle Management (VLM) icon indicates the lifecycle status for the installed version:
|
Latest version | The newest version of software available on the Rockwell Automation Product Compatibility and Download Center. |
Latest patch | The newest software patch available on the Rockwell Automation Product Compatibility and Download Center. |
Activations | The activation search path. |
In FactoryTalk Updater R4.10, it supports checking the OS version of agent both Client and web Client, make sure the installed Agent version is greater than or equal to v4.10 that can collect the OS information and send it to Server.
Checking the OS version of the machine by moving the mouse over the below icon on Client.
Provide Feedback