Find group and add devices for monitoring
- To find machines, select selectFind Machines, and perform one of the following actions:
- To scan the network and find machines automatically, selectAuto Discover.
- To search for machines using an IP address or a range of addresses, selectManual.
- To search for a specific machine, selectSingleand enter the machine's IP address.
- To search for machines within a range of IP addresses, selectRangeand enter the range of IP addresses.
- To locate machines that are not connected to the current server, selectFind Machines.The found machines appear in a table that lists each machine's name and IP address. Found machines are Ungrouped by default.
- To assign a machine to an existing group, select the menu icon
beside the group name and select a group.
Machines left ungrouped appear only in the All Machines list.TIP: To add multiple machines to the same group, select the checkboxes for the machines, select the menu iconin the Group column, and select a group.
- To assign a machine to an existing group, select the menu icon
beside the group name and select +, type the group name and press Enter.
- To add machines to the main page, select the checkbox for the machines and selectAdd Machines.
- To edit a group name or delete a group, select the menu icon
in the Group column, hover over a group, and select the Edit icon
to edit the group name or select the Delete icon
to delete the group.
All machines in a deleted group revert to Ungrouped.
Provide Feedback