Firewall ports and URL access
To ensure FactoryTalk Updater can access the Product Compatibility and Download Center (PCDC) data and download the latest patches, you must add the following URLs to the firewall exception list:
When using the server installation:
- api.rockwellautomation.com
When using the client installation:
- idp.rockwellautomation.com
- netstorage.rockwellautomation.com
Port Type | Port Number | Description |
---|---|---|
TCP | 808 | Allows the Updater agent and client to connect to the Updater server. |
TCP | 60129 | Allows access to the web-based FactoryTalk Updater client. |
UDP | 137 | Used to ping computer names. |
Network-Echo Request (ICMPv4-In) | Allows one computer to contact or ping another computer to test network communications. |
Port Type | Port Number | Description |
---|---|---|
TCP | 30064 | Allows access to the agent service to change the server address. |
UDP | 3702 | Allows Auto Discovery broadcast message. |
UDP | 137 | Used to ping computer names. |
Network-Echo Request (ICMPv4-In) | Allows one computer to contact or ping another computer to test network communications. |
Provide Feedback