Scan for updated information

Scan the server for updated information on machines and activations
  • If you want to manually perform a scan, click
    Scan
    .
  • If you wan to schedule scans at regular intervals, perform the following actions:
    1. On the main menu bar, select
      Schedule
      .
    2. In the
      Schedule
      dialog box, enter the interval (in days) at which scans should occur.
      If you want scans to occur daily, enter
      1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.