force-off-command

Force Off command

Choose this command to force a selected bit OFF. If the bit is part of a SINT, INT, or DINT, only this bit is affected by the force operation.
This command is enabled only if the selected bit is forceable, and either does not currently contain a force or is forced ON.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal