Faceplate Control - Font

Faceplate Control - Font

Use this tab to define the fonts that appear on the faceplates. From here, you can configure a ControlFont to be used in the main part of the faceplate, and a MinorFont to be used in scales and other minor portions of the faceplate.
Parameters
Property Name
Choose the font you want to configure from the pull-down menu. Choose from ControlFont or MinorFont; the default is ControlFont.
Font
Choose the font you wish to use for the control from the list of available fonts. The default font is Arial.
Style
Choose the style you wish to use for the control from the pull-down menu. The default style is Regular.
Size
Enter the point size you wish to use for this font. The default size of the ControlFont is 10.5 points; the default size of the MinorFont is 8.25 points.
Strikeout
Check this box if you want to use the strikeout effect, which draws a line through the font. This option is unchecked, by default.
Underline
Check this box if you want to use the underline effect, which draws a line below the font. This option is unchecked, by default.
OK
Click this button to accept your edits and close the Faceplate Control Properties dialog.
Cancel
Click this button to cancel your edits and close the Faceplate Control Properties dialog.
Apply
Click this button to apply your edits and continue editing in the Faceplate Control Properties dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.