Discover Module command
Add a module from a list of modules attached to a given backplane or network. When selected, the
Module Discovery
tab in the Select Module
dialog box appears.
TIP:
The
Discover Module
command is available only when the Logix Designer
application is online and the network path is valid.Provide Feedback