Open/Import Project Dialog Box
Use this dialog box to open a project file or to perform a full import of a project file. Closes an open project if no changes were made. If the currently open project was modified, a prompt appears to save changes.
Select
Source Control
on the Places toolbar (right portion of the dialog box) to view the AssetCentre Archive source control. Parameters
Parameter | Description |
---|---|
Look in: | Select the directory in which the project resides. |
Up One Level | Move up one level in the directory tree. |
Create New Folder | Create a new folder in the current directory. |
List | Display a list of files in this directory. |
Details | Display a list of files in this directory with all of the associated file details (for example, file size, date). |
File name: |
|
Open/Import | Open or import the specified file. |
Cancel | Cancel the open or import and close the Open/Import Project dialog box. |
Help | View help about Open/Import Project dialog box. |
Source Control View | View the Source Control view. |
Look in: | Select the directory in the AssetCentre archive where the file to import resides. |
Up One Level | Move up one level in the directory tree. Active when logged in to a server or database and not already at the top level of the tree. |
This button is View Menu | Select view type (list of file names or file names with the username). Active when logged in to a server or database. |
Login | Log in to a specific server and attach to a specific database. |
Manage Server Registrations | Open a dialog box to manage one or more server or database combinations. |
Select Version of Label for the Operation | Select an archived element based on either version or a label. Active when a file is selected. |
Search for Files or Folder | Search for files or folders within the current archive database. Active when logged in to a server or database |
Help | View Help about using source control. |
Check Out | If unselected, retrieves a copy of the selected file when clicking Get If selected, checks out the file to retrieve. If selected file is checked out, option is not selected and not active . |
File Name | Displays the currently selected file (read-only). |
Files of type: | Shows the file type. The only available type for the Source Control View is Logix Designer application (.ACD). |
Get | Retrieve the file or determine if file is checked out. This button is active if logged in to a server or database and if have selected a file to retrieve. |
Cancel | Cancel the open or import and close the Open/Import Project dialog box. |
Help | View Help on the Open/Import Project dialog box |
Provide Feedback