Paste command
Paste the contents of the Clipboard at the selected location.
For project documentation, these items apply for the paste command:
- If the project where the product documentation is pasted is language-neutral, the current or default language is pasted into the project.
- If language switching is enabled in the project where project documentation is pasted, then all project documentation retains the language to which it belongs. This may result in project documentation content appearing in the project for a language that previously had no content.
- If language-neutral project documentation is pasted into a project that has a current language, the neutral project documentation is added to the current language (and is no longer neutral project documentation).
When using the paste command in the Add-On Instruction editor, optionally insert a formatted string as a full parameter. The current contents of the clipboard replace the currently selected row. If a row is not selected, a new row inserts above the selected cell. If copying more than one parameter, the order of the pasted parameters is the same as the copied order. If selecting than one row, the selected rows are replaced by the rows from the clipboard. Paste appears dimmed when no text resides on the clipboard or when a read-only row is selected.
Provide Feedback