Add-On Instruction export

An Add-On Instruction definition may be exported to a
Logix Designer
application .L5X file via the Controller Organizer.
Export of an Add-On Instruction definition may include all referenced Add-On Instructions and User-defined Data Types (also known as dependencies) or may include just the selected Add-On Instruction definition itself. Specify at the time of the export whether to include all referenced definitions with the export.
  • By default, dependencies are not included.
  • If dependencies are included, referenced User-defined Data Types and Add-On Instructions are included in the export file.
  • If dependencies are not included, only the exported Add-On Instruction definition is included in the export file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.