Failed to set Alarm Limit value

Problem attempting to set the Alarm Limit values. The error message indicates these conditions:
The immediate value is out of range
Failed to set ALMA Properties – Configuration tab, Alarm Limit value. The value must fall within the range High High Limit > High Limit > Low Limit > Low Low Limit.
Invalid value for Alarm Limits. Enter a valid value so that High High Limit > High Limit > Low Limit > Low Low Limit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.