Deleting or Going to a Bookmark
Bookmarks are used to quickly skip forward or backwards in your program logic to specific points you mark. To access the
Edit/Goto Bookmark
dialog box, click the View All
or Goto Bookmarks
button on the Bookmark
toolbar.To delete or go to a bookmark:
- From the list of available bookmarks, select the one that you want to edit or go to.
- If you want to jump to this bookmark in your logic, click theGotobutton.
- If you want to remove this bookmark from your logic, click theDeletebutton.
- ClickCloseto close the Edit/Goto Bookmark dialog box.
Provide Feedback