- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Showing/hiding toolbars
The Logix Designer application has a number of toolbars that provide you with one-click access to many of the most common tasks you need to complete.
To show or hide toolbars:
- From theViewmenu, chooseToolbars.TheToolbarsdialog box appears.
- To display a toolbar, select the check box next to its name; to hide a toolbar, clear the check box.
- ClickCloseto close theToolbarsdialog box.
Provide Feedback