- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Controller Properties dialog box - OPC UA
Use the setting on the
OPC UA
tab to turn on OPC UA and to select the controller port on which to enable the OPC UA server.
TIP:
.
OPC UA is only available for controllers with nodes.
Parameter | Description |
---|---|
Enable OPC UA | Turn on OPC UA and then select the port on which to enable the OPC UA server. |
Provide Feedback