Handle fault conditions

Handle fault conditions

The controller has a number of facilities to trap and handle controller faults in the logic. For program faults, write a fault routine that is executed when a fault occurs. For other faults (or faults that are not cleared with a fault routine), configure a Controller Fault Handler program. Also configure a Power-Up Handler program to deal with startup conditions after an abnormal power loss while running.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.