Adjust security settings to allow launch of Logix Designer application from a remote computer
To allow users to launch the
Logix Designer
application from a remote computer, change the default security settings in the FactoryTalk
Network Directory. When users log on remotely and try to launch the application, the user is prompted to
Log On to
After providing the proper credentials, the user is sometimes still unable to log on. This happens because the policy FactoryTalk
.Require computer accounts for all client machines
is enabled by default, and the remote computer is not in the FactoryTalk Directory
computer list.To adjust security settings to allow launch of
Logix Designer
application from a remote computer- Add the remote computer to theFactoryTalkNetwork Directory or
- Change the security policy settingIdentify terminal server clients using the name oftoServer Computer.
For details see
Set up security policies
and Add a computer account
in the FactoryTalk Administration Console
help.
TIP:
In the case where a
FactoryTalk
administrator is logged on to the FactoryTalk
Network Directory and Single Single-on is enabled, the client launches the Logix Designer
application using the active administrator account. For details see Single Sign-on
in the FactoryTalk Administration Console
help.Provide Feedback