Select clock priorities
Override the best master clock algorithm to choose a different grandmaster for these cases:
- Knowledge about the reliability or availability of clocks with similar quality values.
- Avoid the clock choice being based on arbitrary values such as device serial numbers or MAC addresses.
- Avoid the clock choice changing when modules are replaced for maintenance purposes.
In these cases, changing the default priority values can make it easier to predict or control which clock is chosen as grandmaster.
TIP:
For large system where there are only a few devices to avoid using, set the priority values for those devices to greater than 128 (default value) and let the remaining devices (including new, out-of-box devices added later) negotiate normally. If only a few devices are using a grandmaster, set their priority values to less than 128.
To select clock priorities:
- In theController Organizer, right-click the controller and chooseProperties. TheController Propertiesdialog box opens.
- Select theDate/Timetab.
- If it is not already selected, selectEnable Time Synchronization.
- Select theAdvancedbutton. TheController Propertiesdialog box -Advance Time Synctab opens.
- To override the actual clock quality values (Priority 1) or override a tie breaker (Priority 2) between two devices that are equal in clock quality, underLocal Clock, enter or select thePriority 1orPriority 2value.The priority values range from 0 through 255, with zero being the highest priority.
- SelectApply.
Provide Feedback