Equipment Sequence Element buttons

The table describes the purpose of each
Equipment Sequence
Element.
Icon
Icon Name
Description
Step and Transition Pair
Add Step and Transition Pair
Use
Add Step and Transition Pair
Step and Transition Pair to add a step and transition pair. Although added as a pair, you can select and edit each element separately.
Disconnected Step
Add Disconnected Step
Use the
Add Disconnected Step
Disconnected Step to add a step without adding a transition.
Diconnected Transition
Add Disconnected Transition
Use
Add Disconnected Transition
Diconnected Transition to add a transition without adding a step.
Simultaneous Divergence
Add Simultaneous Divergence
Use
Add Simultaneous Divergence
Simultaneous Divergence to create a branch where all linked steps execute simultaneously.
Selective Divergence
Add Selective Divergence
Use
Add Selective Divergence
Selective Divergence to create a divergence for a selective branch. In a selective divergence, only one of multiple paths is executed--the path containing the transition that first evaluates as TRUE.
Simultaneous Convergence
Add Simultaneous Convergence
Use
Add Simultaneous Convergence
Simultaneous Convergence to merge simultaneous execution paths back together.
Selective Convergence
Add Selective Convergence
Use
Add Selective Convergence
Selective Convergence
to merge selective divergent paths back into one execution path in the selective branch.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.