Add a disconnected step
Adding a disconnected step (not connected to a transition) is useful to:
- Replace an existing step.
- Add a step to a structure in which a transition is already present, such as the last step in each branch of a simultaneous convergence.
To add a disconnected step:
- Select in the Sequence Editor workspace, or select on an element to connect to in the sequence diagram.
- On theEquipment SequenceElement toolbar, selectAdd Disconnected Step
.
- (optional) Right-click the existing link and then clickDeleteto remove any existing links from the element connectors.
- Click the connector of the first element to create a link, and then click the connector of the second element to attach the link.
Provide Feedback