Configure imported Equipment Sequence properties

Configure imported Equipment Sequence properties

When an
Equipment Sequence
is imported, the configuration properties on the Details pane of the
Import Configuration
dialog box may require adjustment.
To adjust configuration properties for an imported
Equipment Sequence
:
  1. On the
    File
    menu, select
    Import Component > Equipment Sequence
    .
  2. In the
    Import Equipment Sequence
    dialog box, select the sequence to import.
  3. Select
    Open
    .
  4. In the
    Import Configuration
    dialog box, select the
    Operation
    setting for the import.
    The Operation setting chosen depends on whether the Import Name exists in the project.
    If the Import Name is used as a program name in the project, set
    Operation
    to
    Use Existing
    or
    Overwrite
    .
    If the Import Name is not used in the project, set
    Operation
    to
    Create
    or
    Discard
    .
    • Use Existing
      : Specifies that existing settings in the project are used, not the settings in the imported component.
    • Overwrite
      : Specifies that settings in the import file will overwrite the information in the project file, as long as overwriting is a permitted operation.
    • Create
      : Specifies that a new component is created in the project based on the information in the import file, as long as creation is a permitted operation.
    • Discard
      : Operation defaults to
      Discard
      when do not have adequate security privileges to import the file, or if the import file conflicts with the existing project. If the import file conflicts with the existing project, try changing the
      Final Name
      setting to continue the import. If the import does not complete, check security privileges.
  5. (optional) To change the name of the imported file, or if the imported file name conflicts with the existing project, type a
    Final Name
    for the imported file. By default, the
    Final Name
    is the name of the import file.
  6. (optional) When the
    Operation
    is set to
    Create
    , select the
    Properties
    button to view the basic settings for the imported
    Equipment Sequence
    .
  7. (optional) Select
    Collision Details
    to find differences between the imported file settings and the existing settings.
  8. (optional) In
    Description
    , type a description for the import file. If
    Operation
    is set to
    Use Existing
    or
    Discard
    , the
    Description
    box is not available.
  9. (optional) On the
    Schedule In
    menu, select a program location for the
    Equipment Sequence
    . To unschedule the
    Equipment Sequence
    , select
    Unscheduled
    . To schedule the
    Equipment Sequence
    , select a task.
  10. (optional) On the
    Parent
    menu, select a parent for the imported
    Equipment Sequence
    . Use the
    Parent
    setting to group programs hierarchically in the
    Logical Organizer
    .
  11. (optional) Select
    Inhibit Equipment Sequence
    to prevent the
    Equipment Sequence
    from being owned and commanded by another user or program after it is imported.
  12. (optional) Select
    Preserve existing tag values in offline project
    to prevent tag values in the project from being overwritten by an import the
    Equipment Sequence
    in offline mode. Note that tag values are never overwritten when importing an
    Equipment Sequence
    while online with the controller.
  13. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal