Link two sequence elements together

Links connect the elements in an
Equipment Sequence
diagram.
To create a link between sequence elements:
  1. Hover over the circular port below the sequence element. The port turns green.
  2. Drag a link to the port on the top of the second sequence element. If the elements are in a valid structure, the port turns green.
  3. Stop dragging to complete the link.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.