Sequence links
Links connect the elements in an Equipment Sequence diagram.
You can link elements together in specific ways. If there is a port on the side you want to link with, use the port. If there is no port, try the bar.
- Step bottom port to transition top port
- Step bottom port to simultaneous divergence branch
- Step top port to a transition bottom port
- Step top port to a selective convergence port
- Transition bottom port to step top port
- Transition bottom port to simultaneous divergence port
- Transition top port to a step bottom port
- Transition top port to a selective divergence branch
- Transition bottom port to a step top port
- Transition bottom port to a simultaneous convergence port.
Element links
Links connect steps, transitions, and branching structures.
A link connects the bottom connector of an element to the top connector of a following
element. A link may only be added between elements that are not already connected and in
a valid structure.
The following example shows several links and element connectors.
Item | Name | Description |
---|---|---|
Step connector | Valid connection point | |
Link | Click on a valid connection point to create the link | |
Transition connector | Click a second valid connection point to connect the elements |
Branch links
A sequence branch is a structure within an equipment sequence diagram that permits simultaneous or selective execution of steps.
Item | Description |
Transition bottom port to a simultaneous divergence port. | |
Step bottom port to a selective divergence port. | |
Transition bottom port to a selective convergence branch. | |
Step bottom port to a simultaneous convergence branch. |
Provide Feedback