Delete Equipment Sequence elements
Delete one or more sequence elements from an and the project. Deleting a step or a transition removes the element from the Sequence Editor and the project, and also removes the element backing tag. When deleting a step, step tags are also deleted.
Equipment Sequence
diagram. Deleting a link or a branch structure only removes the element from the Sequence EditorTo delete a sequence element:
- Select one or more sequence elements.
- On the Menu bar, selectEdit > Delete.TIP:Also delete a sequence by:
- Right-click the element and selectDelete.
- Select the element and pressDeleteon the keyboard.
Provide Feedback