- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Merge the selective branch
Merge the selective branch in an
Equipment Sequence
diagram using this procedure.To merge the selective branch:
- Select in the Sequence Editor workspace, or select on an element to connect to in the sequence diagram.
- SelectAdd Selective Convergence
on the Sequence Element toolbar.
- Connect the convergence to a step in the sequence diagram.
- Connect the last transition in each divergent path to the selective convergence.
Provide Feedback