- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Simultaneous convergence
A simultaneous convergence is a branching structure that brings together two or more paths run in parallel into a single path.
IMPORTANT:
The transition below the simultaneous convergence will not evaluate until all steps linked to the simultaneous convergence are active.

Item | Description |
![]() | All paths in a simultaneous branch are execution paths. |
![]() | The simultaneous convergence merges the simultaneous execution paths. |
Provide Feedback