- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Equipment Sequence failures
Failures originate from two sources,
Equipment Phase
s and Equipment Sequence
s. An Equipment Phase
generates a failure by executing a Phase Failure (PFL) instruction, maintained by the Failure attribute. The Equipment Sequence
generates a failure by detecting a problem that impairs its ability to coordinate active sequence elements, maintained by the Internal Failure attribute. A failure propagates up the hierarchy of sequence elements from the point it originated;
Equipment Phase
s notify steps and steps notify the Equipment Sequence
. Failure status is maintained at each of these layers: - TheEquipment Phasebacking tag has a Failure member.
- The step backing tag has a Failure member and an Internal Failure member.
- TheEquipment Sequencebacking tag has a Failure member and an Internal Failure member.
A failure is considered a serious problem that warrants holding the execution of the sequence, all active elements, and any phases to which they are attached until the cause of the failure is corrected. This can occur in either Automatic or Manual mode.
Phase-generated failures
Phase-generated failures are the result of the phase logic executing a PFL instruction. The instruction includes a failure code created and managed by the user. The failure is stored on the Failure member of the phase’s backing tag. The failure is detected by the step, setting the Failure member on the step's backing tag. Finally, the failure on the step is detected by the sequence, setting the Failure member on the sequence.
Sequence-generated failures
Sequence-generated failures are detected by the sequencing engine as it executes. The failure is detected by the step and is stored on the Internal Failure member of the step’s backing tag. That failure is detected by the step, setting the Internal Failure member on its backing tag.
Clear failures
The Clear Failures command resets the failure and internal failure members of the sequence and step backing tags. If a phase failure is being cleared, the
Clear Failures
command is forwarded to the phase. Sequences, like phases, cannot be restarted until all their failures are cleared. Note that if the cause of the failure has not been resolved, the next scan of the Equipment Sequence
engine will likely regenerate the failure.You need to do the following sequence of actions in order to recover from an
Equipment Sequence
failure:- Correct the cause of the failure.
- Clear the failure status from the sequence, step, and phase involved in the failure.
- Restart the sequence.
Provide Feedback