- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Failed to open Data Viewer. Unable to get information from Data Item service.
This prompt appears when trying to open the Data Viewer and the
Logix Designer
application is not synchronized with the Data Item service (View Runtime). The prompt indicates failure to open.Select
Retry
to attempt to synchronize with the Data Item service or select Cancel
.![]() | Tip: The retry can take up to 5 minutes or more to complete. |
Provide Feedback