Function Block Properties Dialog Box - JSR Properties

The Jump to Subroutine (JSR) instruction invokes another routine. When that routine completes, the execution returns to the JSR instruction.
Use the
JSR Properties
tab of the
Function Block Properties
dialog box to set the values for the parameters of the selected JSR instruction.
The following table describes the parameters on the
JSR Properties
tab:
Parameter
Description
Routine
Select a routine name to use for the subroutine to execute in the list, or type a routine name directly into the box.
If online, start a pending edit to modify the routine name.
Tip:
MainRoutine
,
Current Routine
,
and
Phase State Routine
are not valid targets as arguments for a JSR instruction, and do not appear in the
Routine
list.
Input and Output Parameters
Select a tag to use for the parameter from the tag browser in the list, or type a tag name directly into the box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.