Modify an Instruction
The RLL Editor provides assistance when editing an instruction filed . For Data Source (and non-data target) operands, the Ladder Editor provides a combo-box in which to edit. This combo-box provides the component list to enter into the operand field.
For Data Target operands, the Ladder Editor provides normal edit control.
- Select Enter to select the entire operand text and place the edit control’s caret at the end of the operand text.
- Select Enter, double click, or use the menus on an instruction comment or main operand tag description to display the ASCII command line editor while editing the comment or description.
Provide Feedback