PAIM Source Quality settings

PAIM Source Quality settings

Use the
Source Quality
tab on the PAIM Properties dialog box to configure settings for evaluating the input source quality for Process Multi Sensor Analog Input (PAIM) instructions.
To configure Source Quality settings for PAIM instructions
  1. On the instruction in the routine, perform one of these actions:
    • On the Ladder or FBD instruction, select .
    • In the Structured Text editor, right-click the tag name and select
      Configure <tag name>
      .
  2. Select the
    Source Quality
    tab.
  3. Configure these settings:
    Setting
    Description
    Reject an input if its quality is uncertain
    Select the checkbox to reject an input marked as having uncertain quality and accuracy.
    Reject inputs when they are: Outside of rejection region (must have three good inputs)
    Select the checkbox to reject inputs that are more than two standard deviations from the mean.
    Reject inputs when they are: Outside of mean +/-
    Select the checkbox and enter a value in the box to reject an input that deviates from the mean by more than the entered value. Value is in PV units.
    IMPORTANT:
    For the
    Outside of rejection region
    selection to be meaningful, you must enter at least four inputs.
    Calculate output using: Median of good inputs
    Select the checkbox to calculate the final Process Variable as the median of the good (non-rejected) Process Variable inputs.
    Calculate output using: Average of good inputs
    Select the checkbox to calculate the final Process Variable as the average of the good (non-rejected) Process Variable inputs.
    If only two inputs are good, use their:
    • Average
    • Minimum
    • Maximum
    Select the checkboxes to use the input average, the lower of the inputs, or the higher of the inputs as the value of the PV.
    PV source and quality: Generate source and quality
    Select this option to have the instruction determine the input source and quality using the PV input, the PV Uncertain input, and the PVBad input.
    PV source and quality: Pass through connected channel's source and quality value
    Select this option to have the instruction determine the input source and quality using the PV input, the PV Uncertain input, and the PVBad input, plus the PV source and quality (SrcQ) input.
  4. When online with the controller, monitor the
    Device state
    and
    Device issues
    indicators at the bottom left of the dialog box:
    • Device state
      . Displays the current device status: PV good, PV uncertain, or PV bad.
    • Device issues
      . Displays fault conditions: None, Any reject, Min good, Fail, or Configuration error.
  5. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal