PVSD speed reference status
Use the
Speed Reference
tab of the PVSD Properties
dialog box to monitor the status of the Process Variable Speed Drive (PVSD) instruction for speed reference. To monitor the speed reference status of PVSD instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select the arrow next toGeneraland then selectSpeed Reference.
- View the read-only parameters:
- Numeric values. Displays the current value of the input, configuration, or output.
- Device state. When theLogix Designerapplication is online with the controller, the indicator displays the current device state, such as Stopped, Running, Out of service.
- Device issues. When theLogix Designerapplication is online with the controller, the indicator displays fault conditions, such as Drive fault or I/O fault.
- Set the parameter:
- Speed reference operator setting. Type the operator entry of the speed reference (setpoint) to the drive. If the setting requires a signature, this will enforce security from the HMI and disable the setting from the Logix Designer dialog.
- SelectApply.
Provide Feedback