Launch a plug-in

Launch a plug-in

With the proper security credentials, you can launch a plug-in by right-clicking a component in the Controller Organizer or the Logical Organizer and selecting the plug-in from the menu.
To launch a plug-in:
  1. In the Controller Organizer or the Logical Organizer, select a program, routine, task, Add-On Instruction, or User-Defined Data Type supported by your plug-in. The plug-in informs the
    Logix Designer
    application of the components from which it can be launched. Note that you might not be able to launch a plug-in from all components.
  2. Right-click and select
    Plug-Ins > <plug-in>
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal