Fault in standard control or safety task

Fault in standard control or safety task

Select
Yes
to confirm that you want to clear faults for these scenarios.
A fault exists in safety task .
Clearing Safety task faults reinitializes the Safety application. Standard control is running, so clearing faults will restart Safety task execution.
A fault exists in safety task  and in standard control.
Clearing Safety task faults reinitializes the Safety application. The controller keyswitch is in RUN, so clearing faults will restart Safety task and standard control execution.
A fault exists in safety task  and in standard control.
The controller keyswitch is in RUN, so clearing faults will restart standard control execution. A download is required to clear the Safety fault.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal