Change SFC Editor > Display Preferences
Use the
Workstation Options
dialog box to customize the behavior and appearance of the Logix Designer application. The Categories
parameter contains a list of all configurable options categories.To change SFC Editor > Display preferences:
- From theToolsmenu, chooseOptions.
- In theWorkstation Optionsdialog box, click theSFC Editor >Displaycategory.
- To display sheet boundaries in the SFC Editor, select theShow Sheet Boundariescheck box.If selected, when the SFC editor has more than one sheet at a time, a solid line appears in the routine view to indicate the boundaries between sheets. The sheet boundaries represent where page breaks occur when printing the routine. This is based upon the configured sheet size for the routine (on the Sheet Layout tab of the routine properties). Showing the sheet boundaries in the routine view allows positioning elements appropriately so they are not split and printed across multiple pages.
- To display dashed lines in the routine view to indicate the grid boundaries, select theShow Cross Reference Gridcheck box.
- To display free-form comments in the routine editor window, select theShow Text Boxesoption.
- (optional) Configure the text box display settings:
- InJustification choose the alignment for the comments text box, eitherLeft,Right, orCenter.
- Select or clear theWord Wrapcheck box, based on your preferences:If cleared, an SFC text box adjusts its vertical and horizontal size automatically based on the text entered.If selected, determine the size of the text box , which in turn affects where words are wrapped.
- Under theLanguage Element Displayheading, configure the following parameters:
- Select theShow Description Boxescheck box to show element descriptions in the routine window. Clear the box to hide element descriptions.For steps, transitions, and stop elements, use theNever Show Descriptioncommand to turn off descriptions for an individual sequential function chart language element (select theDescription Box Displayoption in the workstation options). However, if theDescription Box Displayworkstation option is turned off, theNever Show Descriptioncommand has no effect.
- IfShow Description Boxesis selected, select theUse Tag Description Display Widthsetting from theApplication Displaycategory check box to limit the text box containing the tag comments to a predetermined line width (a set number of characters per line). This option is useful if using these descriptions with other applications.
- Select theShow Tag Alias Informationoption to show base tag information below an element name that is an alias tag.
- ClickOKto accept the changes and close theWorkstation Optionsdialog, or click any other category to continue configuring the workstation options.
Provide Feedback