- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Step/Action Properties - Action Order
Use
Step/Action Properties - Action Order
to modify the order in which actions appear in the routine, which modifies the order in which they are evaluated.Parameter | Description |
---|---|
Action Evaluation Order | Lists all the actions associated with a step in the order in which they are displayed and evaluated. If no actions are defined for the step, this list is empty. Select individual actions in this list to change their relative position, but you cannot make any changes to the actions themselves (for example, the action names and descriptions are read-only). If an action is unnamed, a question mark (?) appears in the Name column. |
Up/Down buttons | Select to change the position of the selected action in the list. |
Provide Feedback